Why nor flashcan not storage the data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why nor flashcan not storage the data

734件の閲覧回数
lixuhui112
Contributor I

We had designed a custom board based on imx6qsabre-AI , but the nor flash storage the data , the code is

#ifdef CONFIG_MXC_SPI

iomux_v3_cfg_t const ecspi1_pads[] = {

    MX6_PAD_CSI0_DAT4__ECSPI1_SCLK | MUX_PAD_CTRL(SPI_PAD_CTRL),

    MX6_PAD_CSI0_DAT5__ECSPI1_MOSI | MUX_PAD_CTRL(SPI_PAD_CTRL),

    MX6_PAD_CSI0_DAT6__ECSPI1_MISO | MUX_PAD_CTRL(SPI_PAD_CTRL),

    MX6_PAD_CSI0_DAT7__GPIO5_IO25 | MUX_PAD_CTRL(NO_PAD_CTRL),

 

};

void setup_spinor(void)

{

    imx_iomux_v3_setup_multiple_pads(ecspi1_pads,

                     ARRAY_SIZE(ecspi1_pads));

        gpio_direction_output(IMX_GPIO_NR(5, 25), 0);

}

int board_spi_cs_gpio(unsigned bus, unsigned cs)

{

    return (bus == 0 && cs == 1) ? (IMX_GPIO_NR(5, 25)) : -1;

}

#endif

U-Boot 2015.04-14468-gd7d7c43-dirty (Jul 08 2016 - 14:38:47)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 46 C

Reset cause: POR

Board: MX6Q-GWI-SCANNER revA

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   FSL_SDHC: 0

SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]

Boot from USB for mfgtools

Use default environment for                              mfgtools

Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

Hit any key to stop autoboot:  0

Bad Linux ARM zImage magic!

=> sf probe 1

SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB

=> setenv serverip 192.168.23.249

=> setenv ipaddr 192.168.23.111

=> setenv gatewayip 192.168.23.1

=> setenv netmask 255.255.255.0

=> saveenv

Saving Environment to SPI Flash...

SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB

Erasing SPI flash...Writing to SPI flash...done

=> print

baudrate=115200

boot_fdt=try

bootargs=console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off

bootcmd=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript;else else if run loadimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi

bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

bootdelay=1

bootscript=echo Running bootscript from mmc ...; source

console=ttymxc0

emmcdev=2

epdc_waveform=epdc_splash.bin

ethprime=FEC

fdt_addr=0x18000000

fdt_file=imx6q-gwi-scanner.dtb

fdt_high=0xffffffff

gatewayip=192.168.23.1

image=zImage

initrd_addr=0x12C00000

initrd_high=0xffffffff

ip_dyn=yes

ipaddr=192.168.23.111

loadaddr=0x12000000

loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};

loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}

loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}

mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off

mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}

mmcautodetect=yes

mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;

mmcdev=0

mmcpart=1

mmcroot=/dev/mmcblk3p2 rootwait rw

netargs=setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp

netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;

netmask=255.255.255.0

script=boot.scr

serverip=192.168.23.249

update_emmc_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if ${get_cmd} ${update_sd_firmware_filename}; then if mmc dev ${emmcdev} 1; then setexpr fw_sz ${filesize} / 0x200; setexpr fw_sz ${fw_sz} + 1; mmc write ${loadaddr} 0x2 ${fw_sz}; fi; fi

update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if mmc dev ${mmcdev}; then if ${get_cmd} ${update_sd_firmware_filename}; then setexpr fw_sz ${filesize} / 0x200; setexpr fw_sz ${fw_sz} + 1; mmc write ${loadaddr} 0x2 ${fw_sz}; fi; fi

Environment size: 3003/8188 bytes

=>

U-Boot 2015.04-14468-gd7d7c43-dirty (Jul 08 2016 - 14:38:47)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 45 C

Reset cause: POR

Board: MX6Q-GWI-SCANNER revA

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   FSL_SDHC: 0

SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]

Boot from USB for mfgtools

Use default environment for                              mfgtools

Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

Hit any key to stop autoboot:  0

Bad Linux ARM zImage magic!

=> print

baudrate=115200

boot_fdt=try

bootargs=console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off

bootcmd=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript;else else if run loadimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi

bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

bootdelay=1

bootscript=echo Running bootscript from mmc ...; source

console=ttymxc0

emmcdev=2

epdc_waveform=epdc_splash.bin

ethprime=FEC

fdt_addr=0x18000000

fdt_file=imx6q-gwi-scanner.dtb

fdt_high=0xffffffff

image=zImage

initrd_addr=0x12C00000

initrd_high=0xffffffff

ip_dyn=yes

loadaddr=0x12000000

loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};

loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}

loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}

mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off

mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}

mmcautodetect=yes

mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;

mmcdev=0

mmcpart=1

mmcroot=/dev/mmcblk3p2 rootwait rw

netargs=setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp

netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;

script=boot.scr

update_emmc_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if ${get_cmd} ${update_sd_firmware_filename}; then if mmc dev ${emmcdev} 1; then setexpr fw_sz ${filesize} / 0x200; setexpr fw_sz ${fw_sz} + 1; mmc write ${loadaddr} 0x2 ${fw_sz}; fi; fi

update_sd_firmware=if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if mmc dev ${mmcdev}; then if ${get_cmd} ${update_sd_firmware_filename}; then setexpr fw_sz ${filesize} / 0x200; setexpr fw_sz ${fw_sz} + 1; mmc write ${loadaddr} 0x2 ${fw_sz}; fi; fi

Environment size: 2904/8188 bytes

=>

nor flash.png

ラベル(2)
0 件の賞賛
3 返答(返信)

470件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xuhui

for saving environment parameters in spi-nor please check

definition in uboot/include/configs/*board*.h file :

#define CONFIG_ENV_IS_IN_SPI_FLASH

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

470件の閲覧回数
lixuhui112
Contributor I

After testing found that flash memory can be an environment variable, but can not use,such as :

U-Boot 2015.04-14468-gd7d7c43-dirty (Jul 11 2016 - 10:44:31)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 45 C

Reset cause: POR

Board: MX6Q-GWI-SCANNER revA

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   FSL_SDHC: 0

SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]

Boot from USB for mfgtools

Use default environment for                              mfgtools

Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

Hit any key to stop autoboot:  0

Bad Linux ARM zImage magic!

=> setenv serverip 192.168.23.249

=> setenv ipaddr 192.168.23.111

=> setenv gatewayip 192.168.23.1

=> setenv netmask 255.255.255.0

=> setenv ip_dyn no

=> setenv netargs setenv bootargs console=ttymxc0,115200 root=/dev/nfs ip=192.168.23.111 nfsroot=192.168.23.249:/home/lxh/nfsroot/nfs2,v3,tcp

=> setenv bootargs console=ttymxc0,115200 root=/dev/nfs ip=192.168.23.111 nfsroot=192.168.23.249:/home/lxh/nfsroot/nfs2,v3,tcp

=> saveenv

Saving Environment to SPI Flash...

SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB

Erasing SPI flash...Writing to SPI flash...done

=> sf probe

SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB

=> sf read ${loadaddr} 0xc0000 0x10000

SF: 65536 bytes @ 0xc0000 Read: OK

=> md.l ${loadaddr}

12000000: 52091475 64756162 65746172 3531313d    u..Rbaudrate=115

12000010: 00303032 746f6f62 7464665f 7972743d    200.boot_fdt=try

12000020: 6f6f6200 67726174 6f633d73 6c6f736e    .bootargs=consol

12000030: 74743d65 63786d79 31312c30 30303235    e=ttymxc0,115200

12000040: 6f6f7220 642f3d74 6e2f7665 69207366     root=/dev/nfs i

12000050: 39313d70 36312e32 33322e38 3131312e    p=192.168.23.111

12000060: 73666e20 746f6f72 3239313d 3836312e     nfsroot=192.168

12000070: 2e33322e 3a393432 6d6f682f 786c2f65    .23.249:/home/lx

12000080: 666e2f68 6f6f7273 666e2f74 762c3273    h/nfsroot/nfs2,v

12000090: 63742c33 6f620070 6d63746f 6d6d3d64    3,tcp.bootcmd=mm

120000a0: 65642063 7b242076 64636d6d 3b7d7665    c dev ${mmcdev};

120000b0: 6d206669 7220636d 61637365 74203b6e    if mmc rescan; t

120000c0: 206e6568 72206669 6c206e75 6264616f    hen if run loadb

120000d0: 73746f6f 70697263 74203b74 206e6568    ootscript; then

120000e0: 206e7572 746f6f62 69726373 653b7470    run bootscript;e

120000f0: 2065736c 65736c65 20666920 206e7572    lse else if run

=>

then I reboot the uboot :

U-Boot 2015.04-14468-gd7d7c43-dirty (Jul 11 2016 - 10:44:31)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 45 C

Reset cause: POR

Board: MX6Q-GWI-SCANNER revA

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   FSL_SDHC: 0

SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]

Boot from USB for mfgtools

Use default environment for                              mfgtools

Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

Hit any key to stop autoboot:  0

Bad Linux ARM zImage magic!

=> sf probe

SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB

=> sf read ${loadaddr} 0xc0000 0x10000

SF: 65536 bytes @ 0xc0000 Read: OK

=> md.l ${loadaddr}

12000000: 52091475 64756162 65746172 3531313d    u..Rbaudrate=115

12000010: 00303032 746f6f62 7464665f 7972743d    200.boot_fdt=try

12000020: 6f6f6200 67726174 6f633d73 6c6f736e    .bootargs=consol

12000030: 74743d65 63786d79 31312c30 30303235    e=ttymxc0,115200

12000040: 6f6f7220 642f3d74 6e2f7665 69207366     root=/dev/nfs i

12000050: 39313d70 36312e32 33322e38 3131312e    p=192.168.23.111

12000060: 73666e20 746f6f72 3239313d 3836312e     nfsroot=192.168

12000070: 2e33322e 3a393432 6d6f682f 786c2f65    .23.249:/home/lx

12000080: 666e2f68 6f6f7273 666e2f74 762c3273    h/nfsroot/nfs2,v

12000090: 63742c33 6f620070 6d63746f 6d6d3d64    3,tcp.bootcmd=mm

120000a0: 65642063 7b242076 64636d6d 3b7d7665    c dev ${mmcdev};

120000b0: 6d206669 7220636d 61637365 74203b6e    if mmc rescan; t

120000c0: 206e6568 72206669 6c206e75 6264616f    hen if run loadb

120000d0: 73746f6f 70697263 74203b74 206e6568    ootscript; then

120000e0: 206e7572 746f6f62 69726373 653b7470    run bootscript;e

120000f0: 2065736c 65736c65 20666920 206e7572    lse else if run

=> run netboot

Booting from net ...

BOOTP broadcast 1

BOOTP broadcast 2

BOOTP broadcast 3

BOOTP broadcast 4

BOOTP broadcast 5

BOOTP broadcast 6

BOOTP broadcast 7

0 件の賞賛

470件の閲覧回数
lixuhui112
Contributor I

in my uboot/include/configs/borad.h file is such as :

#ifdef CONFIG_SYS_USE_SPINOR

#define CONFIG_CMD_SF

#define CONFIG_SPI_FLASH

#define CONFIG_SPI_FLASH_STMICRO

#define CONFIG_MXC_SPI

#define CONFIG_SF_DEFAULT_BUS  0

#define CONFIG_SF_DEFAULT_CS   1

#define CONFIG_SF_DEFAULT_SPEED 20000000

#define CONFIG_SF_DEFAULT_MODE (SPI_MODE_0)

#define CONFIG_ENV_IS_IN_SPI_FLASH   

#endif

but it's the same than I Turn off the power and  restored my save data is not in spi-nor flash

0 件の賞賛