Why i.MX6ULL do not log in

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why i.MX6ULL do not log in

555件の閲覧回数
FrontMan
Contributor I

Please I am having trouble getting started with my NXP i.MX6ULL board, the user guide is not helping me as it stated that that the board will prompt "Industrio log-in" on the computer screen but I saw nothing of such. Please can anyone help me out with a step by step solution......Thanks.

here is my email also: isong.nathan90@gmail.com 

Enabling IW416 Bluetooth on iMX8MM(UART2) + Linux BS

MYS-6ULX Single Board Computer for Industry 4.0 and IoT Applications @

0 件の賞賛
返信
2 返答(返信)

546件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which version of BSP are you using on your board?

538件の閲覧回数
FrontMan
Contributor I

Well I do not know hot to determine that but here is more info about the board.....

OVERVIEW.

IDO-EVB6Y09 is a development board for NXP i.MX6ULL . It is developed based on the IDO-SOM6Y08 core board. It is equipped with NXP IMX6ULLIEC processor and the maximum frequency can reach 800MHz. Support WIFI Bluetooth module and 4G full Netcom module wireless communication mode, provide dual Ethernet interface, CAN, RS-485, RS-232, USB OTG, TF card, SIM card, LVDS, RGB, TP and audio and other functional interfaces . It can be used as an evaluation board or widely used in various industrial Internet of Things gateways and industrial control equipment.

0 件の賞賛
返信