I see in e.g. the devicetree files for e.g. the SabreSD or Nitrogen6x that the pad control for all the relevant pins for the LCD parallel interface are set to 0x10. Why is that? It means that the SPEED field is set to 00 which is reserved according to the reference manual. Is there a particular reason, something I've overlooked or just an error..?
pinctrl_ipu1: ipu1grp {
fsl,pins = <
MX6QDL_PAD_DI0_DISP_CLK__IPU1_DI0_DISP_CLK 0x10
...
解決済! 解決策の投稿を見る。
yes, pad controls of the Dual/Quad are similar to Solo/Duallite
and next Solo/Duallite RM will be updated with this info.
~igor
Hi ThomasG1z
setting Speed 00 LOW — Low frequency (50 MHz)
according to i.MX6DQ RM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I see now that the documentation has been changed from the 2013 to 2014 version currently listed on your site. However for the i.MX6S/DL the reference manual on your web pages are still from 2013 and the speed field is documented like this:
But I assume the pad controls of the Dual/Quad are similar to Solo/Duallite so this field is not really reserved??
yes, pad controls of the Dual/Quad are similar to Solo/Duallite
and next Solo/Duallite RM will be updated with this info.
~igor