Why VDDHIGH_IN power up before VDDARM and VDDSOC for i.MX6QuadPlus compare to i.MX6Quad SABRE AI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why VDDHIGH_IN power up before VDDARM and VDDSOC for i.MX6QuadPlus compare to i.MX6Quad SABRE AI?

Jump to solution
616 Views
m_c
Senior Contributor I

In the i.MX6Quad SABRE AI, VDDHIGH_IN power up after VDDARM and VDDSOC.

In the i.MX6QuadPlus SABRE AI, VDDHIGH_IN power before VDDARM and VDDSOC.

Why?

Labels (1)
0 Kudos
1 Solution
504 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

VDDHIGH_IN powers regulators as shown on Figure 50-1. Power system overview

i.MX6DQ Reference Manual, powering it first provides more smooth power-up sequence.

So later i.MX6QuadPlus design use this option. Datasheet describes power-up sequence as follows:

"Power-Up Sequence - For power-up sequence, the restrictions are as follows:
• VDD_SNVS_IN supply must be turned ON before any other power supply. It may be connected
(shorted) with VDD_HIGH_IN supply."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
504 Views
art
NXP Employee
NXP Employee

Since the VDD_HIGH_IN power rail supplies the on-chip LDO_1P1 voltage regulator that, in turns, supplies the 24MHz oscillator circuit, better is to apply VDD_HIGH_IN first (after or together with VDD_SNVS_IN) during the power-up sequence to provide enough time for the 24MHz oscillator for getting up and running stable before POR_B is released.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
505 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

VDDHIGH_IN powers regulators as shown on Figure 50-1. Power system overview

i.MX6DQ Reference Manual, powering it first provides more smooth power-up sequence.

So later i.MX6QuadPlus design use this option. Datasheet describes power-up sequence as follows:

"Power-Up Sequence - For power-up sequence, the restrictions are as follows:
• VDD_SNVS_IN supply must be turned ON before any other power supply. It may be connected
(shorted) with VDD_HIGH_IN supply."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos