Old BSP with kernel 4.1.15
============
&rpmsg{
compatible = "fsl,imx6sx-rpmsg";
reg = <0x9FFF0000 0x8000>;
status = "okay";
};
New BSP with kernel 5.4
============
&rpmsg{
vdev-nums = <1>;
compatible = "fsl,imx6sx-rpmsg";
reg = <0x9FFF0000 0x10000>;
status = "okay";
};
Query:
================
1) Why RPMSG size change on A9 core only? Does it not required on M4 side as well?
2) What is the calculation to change size from 0x8000 to 0x10000?
Solved! Go to Solution.
Hi rakesh_patel
usually for bsp changes no additional documents provided except on official nxp linux link:
Also nxp official L4.1.15 bsp (from codeaurora.org/external/imx/linux-imx repository) has not such entry :
Old BSP with kernel 4.1.15
============
&rpmsg{
compatible = "fsl,imx6sx-rpmsg";
reg = <0x9FFF0000 0x8000>;
status = "okay";
};
Best regards
igor
Hi rakesh_patel
size may affect transfer rate from M4 to A7. For changes one can refer to:
Best regards
igor
Thanks for sharing the open-forum links.
But, I want some useful information from NXP's documents for changing size in A9 core in new BSP and no change in M4 side.
Please do needful for the same.
Hi rakesh_patel
usually for bsp changes no additional documents provided except on official nxp linux link:
Also nxp official L4.1.15 bsp (from codeaurora.org/external/imx/linux-imx repository) has not such entry :
Old BSP with kernel 4.1.15
============
&rpmsg{
compatible = "fsl,imx6sx-rpmsg";
reg = <0x9FFF0000 0x8000>;
status = "okay";
};
Best regards
igor