Hi All,
I am working in linux terminal to brinup the imx6qsabresd board. i downloaded the fsl-arm-yocto-bsp ( imx-3.10.17-1.0.0_ga ).
While giving bitbake core-image-base ,i am getting below mentioned exception errors :::
test@test:/Thanaraj/linux-android/fsl-release-bsp/build$ bitbake core-image-base
WARNING: Host distribution "Ubuntu-14.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
WARNING: Host distribution "Ubuntu-14.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |###########################################| Time: 0:00:00
Loaded 2005 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.26.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qsabresd"
DISTRO = "poky"
DISTRO_VERSION = "1.5.1"
TUNE_FEATURES = "armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU = "vfp-neon"
meta
meta-yocto = "(nobranch):bee7e3756adf70edaeabe9d43166707aab84f581"
meta-oe = "(nobranch):eb4563b83be0a57ede4269ab19688af6baa62cd2"
meta-fsl-arm = "(nobranch):af392c22bf6b563525ede4a81b6755ff1dd2c1c6"
meta-fsl-arm-extra = "(nobranch):07ad83db0fb67c5023bd627a61efb7f474c52622"
meta-fsl-demos = "(nobranch):5a12677ad000a926d23c444266722a778ea228a7"
meta-fsl-arm
meta-fsl-demos = "(nobranch):fd639897114c09d5146ea1399c16308edfd0108b"
meta-browser = "(nobranch):fc3969f63bda343c38c40a23f746c560c4735f3e"
meta-gnome
meta-networking = "(nobranch):eb4563b83be0a57ede4269ab19688af6baa62cd2"
NOTE: Preparing RunQueue
ERROR: An uncaught exception occured in runqueue, please see the failure below:
ERROR: Running idle function
Traceback (most recent call last):
File "/usr/local/lib/python2.7/dist-packages/bb/runqueue.py", line 1144, in RunQueue._execute_runqueue():
else:
> self.start_worker()
self.rqexe = RunQueueExecuteScenequeue(self)
File "/usr/local/lib/python2.7/dist-packages/bb/runqueue.py", line 1011, in RunQueue.start_worker():
self.teardown = False
> self.worker, self.workerpipe = self._start_worker()
File "/usr/local/lib/python2.7/dist-packages/bb/runqueue.py", line 964, in RunQueue._start_worker(fakeroot=False, rqexec=None):
else:
> worker = subprocess.Popen(["bitbake-worker", magic], stdout=subprocess.PIPE, stdin=subprocess.PIPE)
bb.utils.nonblockingfd(worker.stdout)
File "/usr/lib/python2.7/subprocess.py", line 710, in Popen.__init__(args=['bitbake-worker', 'decafbad'], bufsize=0, executable=None, stdin=-1, stdout=-1, stderr=None, preexec_fn=None, close_fds=False, shell=False, cwd=None, env=None, universal_newlines=False, startupinfo=None, creationflags=0):
c2pread, c2pwrite,
> errread, errwrite)
except Exception:
File "/usr/lib/python2.7/subprocess.py", line 1327, in Popen._execute_child(args=['bitbake-worker', 'decafbad'], executable='bitbake-worker', preexec_fn=None, close_fds=False, cwd=None, env=None, universal_newlines=False, startupinfo=None, creationflags=0, shell=False, to_close=set([16, 15]), p2cread=14, p2cwrite=15, c2pread=16, c2pwrite=17, errread=None, errwrite=None):
child_exception = pickle.loads(data)
> raise child_exception
OSError: [Errno 2] No such file or directory
Am i doing anything wrong?
How to fix this exception errors ?
Any Solution???
已解决! 转到解答。
Hi Gusarambula,
Thanks for reply. That error was cleared by giving
$ bitbake core-image-minimal (This will include all core-image features)
Then i gave ,
$ bitbake core-image-base
Its working properly.
Thanks,
Raj.
Hello Raj kamsani,
Are you still encountering these errors while baking?
I couldn’t reproduce the error. I am using Ubuntu 12.04, which would be the only difference I see. BB_Version is also different but this may be because of the difference in Host version. Have you tried doing a new repo sync from the imx-3.10.17-1.0.0_ga BSP git?
Regards,
Hi Gusarambula,
Thanks for reply. That error was cleared by giving
$ bitbake core-image-minimal (This will include all core-image features)
Then i gave ,
$ bitbake core-image-base
Its working properly.
Thanks,
Raj.