Which pin to use for USB1_ID on i.MX 8M Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which pin to use for USB1_ID on i.MX 8M Mini

1,491 Views
peterlischer
Senior Contributor I

According to the muxing options, the i.MX 8M Mini has a dedicated ID pin for the USB OTG called USB1_ID. This pin does not have any further muxing options. There is also a USB1_OTG_ID function available on the GPIO1_IO10 pin as ALT1 mode. 

What is the difference between these two pins? Which one should be used for a USB 2.0 OTG implementation?

0 Kudos
1 Reply

1,376 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  The following may be helpful:

https://community.nxp.com/message/1161746 

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos