Which peripheral bus controllers are connected via SPBA on iMX6 SL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which peripheral bus controllers are connected via SPBA on iMX6 SL?

跳至解决方案
2,343 次查看
antonb21
Contributor II

Hello All,

I've tried to find which peripheral bus (UART, SPI etc) controllers are connected via SPBA (Shared Peripheral Bus Arbiter) in Freescale documentation. There is no exact list in Reference manual. The only useful information is provided in IMX6DQRM.pdf. And this document is for iMX6 Q/DL chip. The "Figure 58-1. i.MX 6Dual/6Quad SPBA connectivity" in SPBA section showing UART1, ECSPI1-5, AUDMUX, ESAI, SSI1-3, ASRC as peripherals connected to SPBA. This is 14 devices in total. This is also indirectly confirmed in SDMA section saying "An internal peripheral bus connected to the Shared Peripherals Bus Interface (SPBA) that enables access to up to 14 shared peripherals."

I need this information to properly enable/disable SPBA clock for peripherals connected via SPBA.

Best Regards,

Anton

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
1,672 次查看
fabio_estevam
NXP Employee
NXP Employee

Take a look at the imx6sl.dtsi file:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6sl.dtsi?h=imx...

Search for spba and then you can find the peripherals that are connected to it.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,672 次查看
Yuri
NXP Employee
NXP Employee

  You may look at Figure 1-2 (Simplified Block Diagram) of the i.MX6 SL Reference Manual.

For more details please refer to Table 2-5 (SDMA peripheral memory map)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,672 次查看
antonb21
Contributor II

Thank you for reference to memory map. It's actually contains another 2 tables: Table 2-2 (AIPS1 MM) and Table 2-3 (AIPS2 MM). It's differs between iMX6 SL and Q. The only way to access Shared Peripherals are via AIPS1 for SL variant. Table 2-2 says it's accessed via SPBA. But iMX6Q has both AIPS1 and AIPS2 with Shared Peripherals. AIPS1 is similar to SL. AIPS2 looks like direct access for the rest of Shared peripherals.

1,673 次查看
fabio_estevam
NXP Employee
NXP Employee

Take a look at the imx6sl.dtsi file:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6sl.dtsi?h=imx...

Search for spba and then you can find the peripherals that are connected to it.

0 项奖励
回复
1,672 次查看
antonb21
Contributor II

So the right list is:

For iMX6SL these peripherals are accessed via SPBA: UART 1-5, ECSPI 1-4, SPDIF, SSI 1-3

For iMX6Q/DL these peripherals are accessed via SPBA: UART 1, SSI 1-3, ASRC, ESAI, SPDIF, ECSPI 1-5;

   and UART 2-5 are accessed directly.

0 项奖励
回复