Which parts is the 792MHz max stable CPU operation freq applied to

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which parts is the 792MHz max stable CPU operation freq applied to

ソリューションへジャンプ
747件の閲覧回数
anguschen
Contributor II

Hello, team.

According to the IMX6DQRM, the ARM_CLK_ROOT default freq is 792 MHz, but the i.MX6D  have many parts such as:

MCIMX6D4AVT0N8AD cpu max operation freq is 850
MCIMX6D4AVT1N0AD cpu max operation freq is 1000

So, the 792MHZ is applied to the 850MHz part or 1000Mhz part? If the SOC run at 792MHz, Can I select the
850MHz part? After all the MCIMX6D4AVT0N8AD is 4 dollars cheaper than the MCIMX6D4AVT1N0AD .

Thank you!

ラベル(6)
0 件の賞賛
1 解決策
662件の閲覧回数
art
NXP Employee
NXP Employee

There are various i.MX6Dual parts, qualified for different maximum operational frequencies. Refer to the corresponding Data Sheet document to find maximum operational frequency for a particular part number. The latest Rev.5 data sheets are available on the processor's Documentation web page:

https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...

By default, the core clock runs at 792MHz for all parts. Then, it can be changed in software to the maximum allowed frequency for a particular part.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
662件の閲覧回数
anguschen
Contributor II

Thank you!

0 件の賞賛
663件の閲覧回数
art
NXP Employee
NXP Employee

There are various i.MX6Dual parts, qualified for different maximum operational frequencies. Refer to the corresponding Data Sheet document to find maximum operational frequency for a particular part number. The latest Rev.5 data sheets are available on the processor's Documentation web page:

https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...

By default, the core clock runs at 792MHz for all parts. Then, it can be changed in software to the maximum allowed frequency for a particular part.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛