Hello:
I have a imx6ul-evk demo board, now, I want to build a linux platform on it. but I don't want to use yocto to build the kernel. So, I need download the kernel from Freescale Public GIT .
first, I get the kernel from "git://git.freescale.com/auto/linux.git", I can't find some *.dts files about imx6ul. and also, it cause some problem while starting the kernel.
the question is : if I use imx6ul,and use linux-4 version, where I can find the suitable kernel?
TKS
I find the root cause, the source code should git clone from git://git.freescale.com/imx/linux-2.6-imx.git. I select "linux-2.6-imx-rel_imx_4.1.15_1.2.0_ga".
if using imx6ul board, you should modify the defconfig file, because the default setting of CONFIG_SOC_IMX6UL is no, change it to yes.
so the kernel can bring up.
Follow the attached document to build a custom image for your i.MX6UL EVK board.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------