Which ECC i.MX6 ROM code uses?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which ECC i.MX6 ROM code uses?

3,333 Views
simonlie
Contributor I

Hello,

I'm using a i.MX6 Solo processor on a custom board. For my bachelor thesis I need to know which ECC the i.MX6 can handle. I want to boot MLO / Barebox from NAND flash. And don't know which ECC I have to provide the MLO / Barebox with. For example, the same problem I had to do for AM335x and there the ROM code uses BCH8.

Maybe somebody know the awnser or can me link a document. In the official Technical Manual i couldn't find any information about it.

Regards,

Simon

Labels (3)
0 Kudos
Reply
3 Replies

2,815 Views
simonlie
Contributor I

Thank you for the C Code but this is not exactly what I need.

I need to know which ECC the i.MX6 wants to see if it tries to boot from NAND flash. If it is not always the same, where can I get this information from? I think it must be something like Hamming (1-Bit ECC) or BCH(4-40 Bit ECC).

0 Kudos
Reply

2,815 Views
Yuri
NXP Employee
NXP Employee

Please take a look at Chapter 17 [40BIT Correcting ECC Accelerator (BCH)] of the i.MX6 DQ Reference Manual.
The i.MX6 NAND controller (GPMI) uses it.

0 Kudos
Reply

2,815 Views
JerryFan
NXP Employee
NXP Employee

Hi Simon,

i.MX6SL BootROM use different ECC level for FCB(Firmware Config Block) and firmware(such as uboot). For FCB, it is Hamming, and 8 copied of FCB can be supported at most. For firmware, the ECC level can be configured in FCB, the max level is BCH40.

B.R

Jerry

0 Kudos
Reply