Where is updated documents about 32bit DDR3 Script for 3.10.53 BSP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is updated documents about 32bit DDR3 Script for 3.10.53 BSP?

Jump to solution
1,129 Views
JHY
Contributor IV

I have read below link but can not find board/freescale/mx6q_sabresd/flash_header.S.

Futhermore other files in most of documents are not exist, it is concerned with old BSP, I think.

How to Create i.MX6 32bit DDR3 Script Based on 64bit DDR3 Script

Where is updated documents about 32bit DDR3 Script for 3.10.53 BSP?

Labels (1)
0 Kudos
Reply
1 Solution
766 Views
igorpadykov
NXP Employee
NXP Employee

ddr configured in *.cfg files, like uboot../board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg

so one needs to modify it for 32bit memory configuration

View solution in original post

0 Kudos
Reply
3 Replies
766 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

32bit memory configuration is supported in FSL 3.10.53 BSP

refer to attached Linux Guide sect.5 "Enabling Solo Emulation"

included in L3.10.53_1.1.0_LINUX_DOCS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

766 Views
JHY
Contributor IV

It looks like more setting is needed, because it is a guide of u-boot for i.MX 6Solo on an i.MX 6DualLite SABRE-SD and my sabre board has i.MX 6Quad.

What is missing point for i.MX6 Quad system?

0 Kudos
Reply
767 Views
igorpadykov
NXP Employee
NXP Employee

ddr configured in *.cfg files, like uboot../board/freescale/mx6sabresd/mx6q_4x_mt41j128.cfg

so one needs to modify it for 32bit memory configuration

0 Kudos
Reply