Where is the i.MX6 Platform SDK?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the i.MX6 Platform SDK?

1,053件の閲覧回数
cbrust
Contributor III

The following link appears broken and I cannot find the i.MX6 Platform SDK to which it points.  https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null&Parent_nodeId=133...​​

Has the SDK's name/location changed and is it still available or ... something else?

Thanks in advance.

cliff

ラベル(4)
0 件の賞賛
1 返信

641件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The Platform SDK for i.MX6 was removed since it is not supported more.

Please create SR to get it if needed.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛