Hi community,
I am trying to run a demo of RPMsg with 8MMINILPD4-EVK.
linux is 4.14-sumo and RTOS is FreeRTOS with rpmsg_lite.
The following thread is helpful, but it does not work well.
iMX8QXP: Use RPMSG to wake up M4 and A35
Are there any documents that might be helpful?
And where is the source code of "imx8mm_m4_TCM_rpmsg_lite_pingpong_rtos_linux_remote.bin"?
As far as I checked, it was looping endlessly with rpmsg_ns_announce-> rpmsg_lite_format_message-> vq_tx_remote-> RL_ASSERT.
The value of buffer_len seems to be strange as follows.
[virtqueue_create_static (151)] vq->vq_nentries = 2, vq->vq_ring_size = 4126, vq->vq_ring_mem = 0x90010000
[vring_init (151)] vr->desc = 0x90010000, vr->avail = 0x90010020, vr->used = 0x90011000
[virtqueue_create_static (151)] vq->vq_nentries = 2, vq->vq_ring_size = 4126, vq->vq_ring_mem = 0x90018000
[vring_init (151)] vr->desc = 0x90018000, vr->avail = 0x90018020, vr->used = 0x90019000
[RPMsgTask (100)] rpmsg_lite_remote_init OK (0 msec)
[RPMsgTask (102)] Wating rpmsg_lite_is_link_up (0 msec)
Link is up!
[RPMsgTask (111)] rpmsg_queue_create OK (1990 msec)
[RPMsgTask (118)] rpmsg_lite_create_ept OK (1990 msec)
[virtqueue_get_available_buffer (355)] head_idx = 0, *avail_idx = 18407, *len = 3878398162
buffer = 3D9A5489, buff_len = 3878398162, idx = 18407
[virtqueue_add_consumed_buffer (373)] head_idx = 18407, vq->vq_nentries = 2,
Best Regards,
T.kashiwagi
已解决! 转到解答。
Hi all,
I solved this, and I will post the settings.
About document , please refer to below.
About RTOS sample code , please refer to below.
How to run RPMsg sample is as follows.
Please note that CM4 and kernel modules do not work if they are mismatched.
The procedure is as follows.
1. Please boot linux and "imx8mm_m4_TCM_rpmsg_lite_str_echo_rtos.bin". dmesg will be as follows.
root@imx8mmevk:~# dmesg | grep rpmsg
[ 0.861067] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 0.861114] virtio_rpmsg_bus virtio0: creating channel rpmsg-virtual-tty-channel-1 addr 0x1e
[ 0.873812] imx rpmsg driver is registered.
root@imx8mmevk:~#
2. Please load "imx_rpmsg_tty.ko" ($ insmod imx_rpmsg_tty.ko). RPMsg tty driver is installed (/dev/ttyRPMSG30 appers).
root@imx8mmevk:~# dmesg | grep rpmsg
[ 0.861067] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 0.861114] virtio_rpmsg_bus virtio0: creating channel rpmsg-virtual-tty-channel-1 addr 0x1e
[ 0.873812] imx rpmsg driver is registered.
[ 651.497802] imx_rpmsg_tty virtio0.rpmsg-virtual-tty-channel-1.-1.30: new channel: 0x400 -> 0x1e!
[ 651.506808] Install rpmsg tty driver!
[ 651.512199] rpmsg_tty_cb68 65 6c 6c 6f 20 77 6f 72 6c 64 21 hello world!
root@imx8mmevk:~#
The following message is displayed on the CM4 console at this point.
Nameservice sent, ready for incoming messages...
Get Message From Master Side : "hello world!" [len : 12]
3. you can echo string as follows.
Best Regards,
T.Kashiwagi
Hi all,
I solved this, and I will post the settings.
About document , please refer to below.
About RTOS sample code , please refer to below.
How to run RPMsg sample is as follows.
Please note that CM4 and kernel modules do not work if they are mismatched.
The procedure is as follows.
1. Please boot linux and "imx8mm_m4_TCM_rpmsg_lite_str_echo_rtos.bin". dmesg will be as follows.
root@imx8mmevk:~# dmesg | grep rpmsg
[ 0.861067] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 0.861114] virtio_rpmsg_bus virtio0: creating channel rpmsg-virtual-tty-channel-1 addr 0x1e
[ 0.873812] imx rpmsg driver is registered.
root@imx8mmevk:~#
2. Please load "imx_rpmsg_tty.ko" ($ insmod imx_rpmsg_tty.ko). RPMsg tty driver is installed (/dev/ttyRPMSG30 appers).
root@imx8mmevk:~# dmesg | grep rpmsg
[ 0.861067] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 0.861114] virtio_rpmsg_bus virtio0: creating channel rpmsg-virtual-tty-channel-1 addr 0x1e
[ 0.873812] imx rpmsg driver is registered.
[ 651.497802] imx_rpmsg_tty virtio0.rpmsg-virtual-tty-channel-1.-1.30: new channel: 0x400 -> 0x1e!
[ 651.506808] Install rpmsg tty driver!
[ 651.512199] rpmsg_tty_cb68 65 6c 6c 6f 20 77 6f 72 6c 64 21 hello world!
root@imx8mmevk:~#
The following message is displayed on the CM4 console at this point.
Nameservice sent, ready for incoming messages...
Get Message From Master Side : "hello world!" [len : 12]
3. you can echo string as follows.
Best Regards,
T.Kashiwagi
Hi,
For i.MX8M Mini RPMsg-related documentation, you could refer to the RPMsg information included on the “i.MX Linux Reference Manual” document, included on the “L4.9.123_2.3.0_8MM_GA_LINUX_DOC” package.
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------
Hi Carlos
Thank you for responding.
My current situation is as follows.
・ In RTOS, I was able to load and execute the sample source (rpmsg_lite_pingpong_rtos_linux_remote). However, it will not be executed from "Send Name Service Announcement".
・ In Linux, I can not execute unit_test. There is no "/ dev / ttyRPMsg".
I have read “i.MX Linux Reference Manual” document. I checked kernel config and exectuted "insmod" as follows.
In menu configuration enable the following module:
• Device Drivers > IMX RPMSG pingpong driver -- loadable modules only
• Device Drivers > IMX RPMSG tty driver -- loadable modules only
root@imx8mmevk:/lib/modules/4.14.78-imx_4.14.78_1.0.0_ga+g94da7bdc489b/kernel/drivers/rpmsg# insmod im
x_rpmsg_tty.ko
insmod: ERROR: could not insert module imx_rpmsg_tty.ko: File exists
root@imx8mmevk:/lib/modules/4.14.78-imx_4.14.78_1.0.0_ga+g94da7bdc489b/kernel/drivers/rpmsg#
"imx_rpmsg_tty.ko" appears to be loaded but there is no "/ dev / ttyRPMsg".
Do you know what caused it?
Best Regards,
T.Kashiwagi
Hi all
I changed "RPMSG_LITE_SHMEM_BASE" as follows.
#define RPMSG_LITE_SHMEM_BASE 0xb8000000
and "rpmsg_ns_announce" was executed.
[RPMsgTask (88)] Start (0 msec)
[virtqueue_create_static (151)] vq->vq_nentries = 2, vq->vq_ring_size = 4126, vq->vq_ring_mem = 0xB8000000
[vring_init (151)] vr->desc = 0xB8000000, vr->avail = 0xB8000020, vr->used = 0xB8001000
[virtqueue_create_static (151)] vq->vq_nentries = 2, vq->vq_ring_size = 4126, vq->vq_ring_mem = 0xB8008000
[vring_init (151)] vr->desc = 0xB8008000, vr->avail = 0xB8008020, vr->used = 0xB8009000
[RPMsgTask (101)] rpmsg_lite_remote_init OK (0 msec)
[RPMsgTask (103)] Wating rpmsg_lite_is_link_up (0 msec)
Link is up!
[RPMsgTask (112)] rpmsg_queue_create OK (1980 msec)
[RPMsgTask (119)] rpmsg_lite_create_ept OK (1980 msec)
[virtqueue_get_available_buffer (355)] head_idx = 0, *avail_idx = 0, *len = 512
buffer = 78040000, buff_len = 512, idx = 0
Nameservice announce sent.
Next, I tried to execute "/unit_tests/Remote_Processor_Messaging/mxc_mcc_tty_test.out" according to i.MX_Reference_Manual.
I enabled the following module:
• Device Drivers > IMX RPMSG pingpong driver -- loadable modules only
• Device Drivers > IMX RPMSG tty driver -- loadable modules only
but "/dev/ttyRPMSG30" could not be found. Which tty can I use instead?
Best Regards,
T.Kashiwagi