Hello All,
Where is core-image recipe? If i see core-image-minimal.bb,
SUMMARY = "A small image just capable of allowing a device to boot."
IMAGE_INSTALL = "packagegroup-core-boot ${ROOTFS_PKGMANAGE_BOOTSTRAP} ${CORE_IMAGE_EXTRA_INSTALL}"
IMAGE_LINGUAS = " "
LICENSE = "MIT"
inherit core-image
IMAGE_ROOTFS_SIZE ?= "8192"
So where is it getting all the packages from? If i have to see and edit the packages it is downloading where should i look at??
Please let me know.
Regards,
Manju
Hi Manjunath,
Following links may be helpful:
How to add a new layer and a new recipe in Yocto
Freescale Yocto Project main page
Can we add Debian packages(Package_deb) in Yocto build?
Regards
Hello,
Thanks for reply. I really appreciate the third link you have sent me. But my question was where is the core-image actually?
Means, let me put it this way,
core-image-sato
core-image-x11
core-image-base
core-image-minimal
All the above recipes use "core-image" as inherited common image. I hope you agree. Now, where is that ? I tried to grep but couldn't find.
Regards,
Manju