Where is ADDR_TRANSLATION_SUPPORT_EN set, for the PCIe ATU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where is ADDR_TRANSLATION_SUPPORT_EN set, for the PCIe ATU?

582 次查看
shefft
Contributor IV

Using iMX6Solo - Figure49-24 shows different options for the ATU.  One key selector in the diagram is the ADDR_TRANSLATION_SUPPORT_EN bit.  It is not mentioned by this name anywhere else in the document.  So what is it?  Where to find it?

标签 (1)
0 项奖励
回复
1 回复

443 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The ADDR_TRANSLATION_SUPPORT_EN bit relates to PCIe IP, which is
embedded in i.MX6 SOC, and strictly speaking it should be removed from

i.MX6 Reference Manual.

http://read.pudn.com/downloads153/ebook/670795/DWC_pcie_reference.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复