Where can i get the latest BSP of i.MX6ULL Evaluation Kit , Except for yocto method

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can i get the latest BSP of i.MX6ULL Evaluation Kit , Except for yocto method

836件の閲覧回数
510015320
Contributor I

Because google's link is not avaliable in china ,so yocto project can not use by setting.I need to build uboot and kernel in standalone environment,but i can not  generate it from yocto project. where can i get the latest  BSP of i.MX6ULL Evaluation Kit? Please tell me the github link.

Downloading Repo source from https://gerrit.googlesource.com/git-repo
fatal: Cannot get https://gerrit.googlesource.com/git-repo/clone.bundle
fatal: error [Errno 110] Connection timed out
fatal: cloning the git-repo repository failed, will remove '.repo/repo'

ラベル(1)
2 返答(返信)

719件の閲覧回数
turker
Contributor IV

You can access kernel and bootloader sources from below links:

linux-imx - i.MX Linux kernel 

uboot-imx - i.MX U-Boot 

719件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello HU YUAN,

Please use the repositories suggested by Tahsin Türker Mutlugün.

Additionally, the following document may help on workarounds when working with the Linux BSP.

Compiling L5.4.3_1.0.0 BSP On Ubuntu 180.4 LTS

https://community.nxp.com/docs/DOC-346009 

I hope this helps!

Regards,