Where can i get the latest BSP of i.MX6ULL Evaluation Kit , Except for yocto method

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where can i get the latest BSP of i.MX6ULL Evaluation Kit , Except for yocto method

844 次查看
510015320
Contributor I

Because google's link is not avaliable in china ,so yocto project can not use by setting.I need to build uboot and kernel in standalone environment,but i can not  generate it from yocto project. where can i get the latest  BSP of i.MX6ULL Evaluation Kit? Please tell me the github link.

Downloading Repo source from https://gerrit.googlesource.com/git-repo
fatal: Cannot get https://gerrit.googlesource.com/git-repo/clone.bundle
fatal: error [Errno 110] Connection timed out
fatal: cloning the git-repo repository failed, will remove '.repo/repo'

标签 (1)
2 回复数

727 次查看
turker
Contributor IV

You can access kernel and bootloader sources from below links:

linux-imx - i.MX Linux kernel 

uboot-imx - i.MX U-Boot 

727 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello HU YUAN,

Please use the repositories suggested by Tahsin Türker Mutlugün.

Additionally, the following document may help on workarounds when working with the Linux BSP.

Compiling L5.4.3_1.0.0 BSP On Ubuntu 180.4 LTS

https://community.nxp.com/docs/DOC-346009 

I hope this helps!

Regards,