Where I can find Module.symvers file for kernel 5.10.9-1.0.0+g32513c25d8c7?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where I can find Module.symvers file for kernel 5.10.9-1.0.0+g32513c25d8c7?

1,823 次查看
jasonpowell_2
Contributor III

I have system on i.MX 8M Nano DDR4 Evk board, uname -r

5.10.9-1.0.0+g32513c25d8c7

built from

$ repo init -u git://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-gatesgarth -m imx-5.10.9-1.0.0.xml

Where is Module.symvers file? I expected to see it either on 8M Nano board system or in the yocto folder imx-yocto-bsp.

Thanks for the help.

JP

 

标签 (1)
标记 (2)
0 项奖励
3 回复数

1,817 次查看
joanxie
NXP TechSupport
NXP TechSupport

why do you need Module.symvers file?

0 项奖励

1,810 次查看
jasonpowell_2
Contributor III

Hi joanxie,

The reason why I need Module.symvers files is the following:

I was trying to compile and load driver panel-ilitek-ili9881c which is not present in the system on my i.MX 8M Nano DDR4 EVK:

Linux imx8mnddr4evk 5.10.9-1.0.0+g32513c25d8c7 #1 SMP PREEMPT Tue Mar 9 02:17:18 UTC 2021 aarch64 aarch64 aarch64 GNU/Linux. 

Hence, I have downloaded kernel 5.10.9 from https://cdn.kernel.org/pub/linux/kernel/v5.x/linux-5.10.9.tar.gz and cross-compiled driver to obtain kernel module file panel-ilitek-ili9881c.ko (matching vermagic and .config) on the x86_64 Linux dedicated machine cross-compiled for aarch64 architecture. Then I downloaded panel-ilitek-ili9881c.ko to my  i.MX 8M Nano DDR4 EVK board. When I tried

$ insmod panel-ilitek-ili9881c.ko

I was getting these messages:

[  122.920524] panel_ilitek_ili9881c: disagrees about version of symbol regulator_enable

[  122.928511] panel_ilitek_ili9881c: Unknown symbol regulator_enable (err -22)

[  122.935624] panel_ilitek_ili9881c: disagrees about version of symbol gpiod_set_value

[  122.943455] panel_ilitek_ili9881c: Unknown symbol gpiod_set_value (err -22)

[  122.950459] panel_ilitek_ili9881c: disagrees about version of symbol drm_panel_add

[  122.958078] panel_ilitek_ili9881c: Unknown symbol drm_panel_add (err -22)

[  122.964905] panel_ilitek_ili9881c: disagrees about version of symbol drm_mode_probed_add

[  122.973020] panel_ilitek_ili9881c: Unknown symbol drm_mode_probed_add (err -22)

[  122.980374] panel_ilitek_ili9881c: disagrees about version of symbol mipi_dsi_attach

[  122.988135] panel_ilitek_ili9881c: Unknown symbol mipi_dsi_attach (err -22)

And since versions of symbols are present in the Module.symvers and vmlinux.symvers files I wanted to find original Module.symvers file as per my question to try to compare the symbol CRC values. For instance, the symbol regulator_enable is present in both Module.symvers and vmlinux.symvers files, and I am not sure how to match these symbols versions obtained from cross-compilation to the symbols versions (which I even do not know where to find at this point) on my i.MX 8M Nano board whose system is obtained from:

$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-gatesgarth -m imx-5.10.9-1.0.0....

As a test I also picked random kernel module from cross-compilation, downloaded it to the i.MX 8M nano board and successfully insmod it and rmmod it to the kernel. The issue I have is with panel-ilitek-ili9881c.ko.

Hope I answered your question. Maybe I am missing some steps too?

Thanks.

JP

标记 (3)
0 项奖励

1,747 次查看
joanxie
NXP TechSupport
NXP TechSupport

if you need add new module, when you build the kernel, you can use "bitbake -c menuconfig linux-imx", then choose the module there

0 项奖励