When overlaysink (i.mx8mq) is available??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When overlaysink (i.mx8mq) is available??

569 Views
bcsong
Contributor I

I want to see that four mp4 files(stream) are decoded simultaneously with vpu  ..

And 4 resize video display (overlay) in 1 HDMI monitor.

How can I do ... with mx8mqevk  board ??

Thanks..

0 Kudos
1 Reply

435 Views
b36401
NXP Employee
NXP Employee

You can refer to chapter 7.5 Overlaysink Usage of i.MX Linux User's Guide I attached.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos