What to do with unused NVCC_RGMIIx pin in i.MX6SX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What to do with unused NVCC_RGMIIx pin in i.MX6SX

Jump to solution
521 Views
ko-hey
Senior Contributor II

Hi all

I have a question about NVCC_RGMIIx pin when it's unused.

What to do with NVCC_RGMIIx pin when it's unused ?

Can it be float ?

According to the following thread, it must be powered to unused digital pin.

However, it isn't mentioned for NVCC_RGMIIx pin in datasheet.

https://community.nxp.com/message/548314 

Please tell me what to do with unused NVCC_RGMIIx pin.

Ko-hey

Labels (2)
0 Kudos
1 Solution
415 Views
jimmychan
NXP TechSupport
NXP TechSupport

If the RGMIIx IF is not used, the RGMIIx IF pins together with the corresponding NVCC_RGMIIx could be left floating.

View solution in original post

0 Kudos
1 Reply
416 Views
jimmychan
NXP TechSupport
NXP TechSupport

If the RGMIIx IF is not used, the RGMIIx IF pins together with the corresponding NVCC_RGMIIx could be left floating.

0 Kudos