For the iMX6SDL, the Linux PCIe driver sets the DEVICE_TYPE in GPR12 to 0x4 for RC mode: // set device type to RC (PCI_EXP_TYPE_ROOT_PORT=4 is from pcie_regs.h)
imx_pcie_clrset(iomuxc_gpr12_device_type, PCI_EXP_TYPE_ROOT_PORT << 12, IOMUXC_GPR12
);
This seems odd since the ref manual says that 0x2 is the proper value for RC mode:
0000 PCIE_EP — EP Mode
0010 PCIE_RC — RC Mode
Can anyone explain why that it is? And how it is that it works that way? Wondering what setting I should use for an RTOS version of the driver I'm creating.
已解决! 转到解答。
Tyler,
It is a typo mistake in RM doc, would be fixed in later version. The BSP code is right.
i.MX 6Dual/6Quad Applications Processor Reference Manual
Document Number: IMX6DQRM - Rev. 3, 07/2015
It has being corrected on some of our newer devices, documentation… This has being corrected on our imx6slx documentation as you can see below..
i.MX 6SoloX Applications Processor Reference Manual
Document Number: IMX6SXRM, Rev 0, 2/2015
Best Regards,
Norbel
Follow up question on a similar issue - the LVDS1_CLK_SEL field in the CCM_ANALOG_MISC1 register...
Linux sets this to be 0x8000040B ( so 0b01011 for that field) which is not present in the list:
00000 ARM_PLL — Arm PLL
00001 SYS_PLL — System PLL
00010 PFD4 — ref_pfd4_clk == pll2_pfd0_clk
00011 PFD5 — ref_pfd5_clk == pll2_pfd1_clk
00100 PFD6 — ref_pfd6_clk == pll2_pfd2_clk
00101 PFD7 — ref_pfd7_clk == pll2_pfd3_clk
00110 AUDIO_PLL — Audio PLL
00111 VIDEO_PLL — Video PLL
01000 MLB_PLL — MLB PLL
01001 ETHERNET_REF — ethernet ref clock (ENET_PLL)
01010 PCIE_REF — PCIe ref clock (125M)
01100 USB1_PLL — USB1 PLL clock
01101 USB2_PLL — USB2 PLL clock
01110 PFD0 — ref_pfd0_clk == pll3_pfd0_clk
01111 PFD1 — ref_pfd1_clk == pll3_pfd1_clk
10000 PFD2 — ref_pfd2_clk == pll3_pfd2_clk
10001 PFD3 — ref_pfd3_clk == pll3_pfd3_clk
10010 XTAL — xtal (24M)
10011 LVDS1 — LVDS1 (loopback)
10100 LVDS2 — LVDS2 (not useful)
10101 to 11111 ref_pfd7_clk == pll2_pfd3_clk
Tyler,
Please take a look at latest RM, it shows 01011 as “SATA_REF – SATA ref clock(100M)”
Selection 01011 is associated with SATA on the 6DQ. But SATA doesn't exist on either the 6SDL or the 6SL.
As I understand it if you set the value 01011 it enables the 100Mhz differential clock, even if SATA module is not on device.
Tyler,
It is a typo mistake in RM doc, would be fixed in later version. The BSP code is right.
i.MX 6Dual/6Quad Applications Processor Reference Manual
Document Number: IMX6DQRM - Rev. 3, 07/2015
It has being corrected on some of our newer devices, documentation… This has being corrected on our imx6slx documentation as you can see below..
i.MX 6SoloX Applications Processor Reference Manual
Document Number: IMX6SXRM, Rev 0, 2/2015
Best Regards,
Norbel