Hi there,
I am trying to flash emmc using serial download mode. Below are my observations related to speed of serial download mode.
1) 31248754032 Bytes image is taking 1787 seconds which is 16.67 MB/seconds
2) 31248754032 Bytes image is taking 1778 seconds which is 16.76 MB/seconds
3) 31248754032 Bytes image is taking 1767 seconds which is 16.86 MB/seconds
As per the RM, the ROM code is using USB OTG1 in high-speed mode and so the theoretical speed would be around 480 Mbps (60 MBps). But in the case of iMX8MQ, I am observing an average speed which is around 16.76 MBps.
Can someone suggest to me how can I increase the speed or what is the maximum speed supported by imx8mq in serial download mode?
Many Thanks,
Ranjitsinh Rathod