Hi community,
I have a question about gstremaer1.0 in i.MX6 Linux BSP.
I want to use imxvideoconvert_g2d gstremer1.0 element to resizing.
Then, I tried some elements with imxvideoconvert_g2d (e.g. imxv4l2src, ximagesrc) on L3.10.53_1.1.0-ga BSP, but it was failed with error such as the following message.
WARNING: erroneous pipeline: could not link imxv4l2src0 to imxvideoconvert_g2d0
Then, would you let me know what element is able to be used with imxvideoconvert_g2d0?
Best Regards,
Satoshi Shimoda1.
解決済! 解決策の投稿を見る。
Hi Satoshi
please refer to attached Linux Guide sect.7.5.4 Video Conversion
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
please refer to attached Linux Guide sect.7.5.4 Video Conversion
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Yes, according to the document, I can understand videotestsrc elements can be used for source of imxvideoconvert_g2d.
Is that all?
Or can I use other element also for imxvideoconvert_g2d?
Actually, I want to use imxvideoconvert_g2d resizing of camera input.
But videotestsrc is not camera input I think.
Best Regards,
Satoshi Shimoda
Hi Satoshi
yes this all
Best regards
igor
Hi Igor,
OK, I understood.
Thank you for your support
Best Regards,
Satoshi Shimoda