What are type and pin assignment of JTAG connector (J4) on i.MX 8QuadXPlus MEK(MCIMX8QXP-CPU)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are type and pin assignment of JTAG connector (J4) on i.MX 8QuadXPlus MEK(MCIMX8QXP-CPU)?

2,642件の閲覧回数
takashisone
Contributor II

I'd like to connect Lauterbach JTAG debugger to the JTAG connector (J4) on i.MX 8QuadXPlus MEK(MCIMX8QXP-CPU) to debug CA35 software, and I'd like to know the connector type and pin assignment for JTAG signal.

ラベル(1)
5 返答(返信)

2,557件の閲覧回数
rweiss
Contributor V

Hello Takashi san,

the pinout of this board is MIPI-10 compatible. You can adapt from the standard 20-pin header to MIPI-10 using the adapter LA-3770.

Product description is here: TRACE32® Converter ARM-20 to MIPI-10/20/34 Arm

ad3770.jpg

0 件の賞賛

2,557件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi Takashi,

Please refer below image for JTAG pinout and connector part# as well for J4.

pastedImage_1.png

Regards,

Mrudang

2,557件の閲覧回数
takashisone
Contributor II

Hello Mrudang,

Thank you very much for the information.
If it's possible, could you please let me know where you had the schematic ?
Regards,
Takashi

0 件の賞賛

2,557件の閲覧回数
mrudangshelat1
Senior Contributor II

HI Takashi,

The design files are available online.

i.MX 8QuadXPlus Multisensory Enablement Kit | NXP 

Regards,

Mrudang

2,557件の閲覧回数
takashisone
Contributor II

Hello Mrudang,
Thank you very much.
I could find a zip file on the URL that includes schematic and BOM.
Regards,
Sone