Weston failing to restore screen properly after being put on standby on imx8mq/mm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Weston failing to restore screen properly after being put on standby on imx8mq/mm

485件の閲覧回数
asabil
Contributor I

Hi,

We have noticed that the 4.14.78 and 4.14.98 BSP release from NXP for the imx8mq/mm applies a patch to set the idle-time to 0 in Weston. This patch effectively stops Weston from ever putting the screen on standby.

When changing this timeout to a positive value, to enable screen standby after a set timeout, we experience that the screen either never wakes up, or wakes up with an offset image wrapping around horizontally and with mixed up colors.

Is screen standby in Weston not supposed by the BSP release from NXP?

Thanks,

Ali

ラベル(1)
0 件の賞賛
1 返信

411件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Ali,

Sorry this marked as a bug, since screen standby is not supported by Weston yet, Hopefully we will integrated in next release.

Regards

0 件の賞賛