Hello,
What do you think of using the imx internal watchdog timer with fsl,ext-reset-output dts property to output reset signal to PMIC ?
Is it safe enough, and guaranteed that the Low frequency reference clock feeding the WDOG block doesn't stop in case of hanging ?
Or perhaps should I use an hardware reset handler ?
Hi matt67
yes using internal watchdog to reset pmic is fine solution and it is safe.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi matt67
yes it is safe also in u-boot.
Best regards
igor