Hi,
I'm working on a device that has iMX7D on it. We will use the LPSR mode, and I have a specific question related to waking up iMX7D from LPSR mode.
The reference manual says that gpio1_io00 .. gpio1_io15 can be used for waking up the processor.
Does it mean that these pads can wake up the processor only when muxed as "pure GPIO"?
If I have pads T2 (gpio1_io12) and T3 (gpio1_io13) multiplexed as FlexCAN RX and TX, would any activity on these pads wake up the processor?
Thanks & best regards,
Jari Peltonen
Hi Igor,
Thanks for your message!
This then means that a separate wake-up signal is needed if CAN Bus is supposed to wake up the processor.
I have no further questions at this point, so we can close this thread.
Best regards,
Jari
Hi Jari
>If I have pads T2 (gpio1_io12) and T3 (gpio1_io13) multiplexed as FlexCAN RX and TX,
>would any activity on these pads wake up the processor?
I am afraid no, they should be configured as gpios.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------