Wake-up from suspend by UARTs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wake-up from suspend by UARTs

956 Views
enginlee
Contributor II

Hi,

I found a strange issue on my i.MX6ULL board:

There is a MCU connect to CPU with UART3, and UART2 is unused.

Application access ttymxc2 without any problem, and also set "enabled" to "/sys/class/tty/ttymxc2/power/wakeup".

But after suspend to RAM (echo mem > /sys/power/state), ttymxc2 becomes abnormal, I cannot read/write anymore.

And I can see the power consumption during suspend mode is higher than it should be, about 10% increase.

I tried lots of settings (BSP/USB/SAI/GPIOs), and finally I found a solution: set "enabled" to "/sys/class/tty/ttymxc1/power/wakeup".

Even through there is no signal connect to UART2, but it just working: ttymxc2 works fine after waking up, and power consumption is normal.

I am not sure the reason why it happened, but I can reproduce this issue on both SDKs (4.14.78_ga_1.0.0 and 4.14.98_ga_2.0.0)

Thanks,

-Engin

Labels (3)
0 Kudos
Reply
2 Replies

847 Views
igorpadykov
NXP Employee
NXP Employee

Hi Engin

>But after suspend to RAM (echo mem > /sys/power/state), ttymxc2

>becomes abnormal, I cannot read/write anymore.

in suspend state uart is not intended to operate and

if it receives data it will cause processor to exit from low power mode.

Also if uart clocks are gated in low power mode (using CCM_CCGRn)

it is not possible to read uart registers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

847 Views
enginlee
Contributor II

Very USEFUL answer!!! HAHAHA

0 Kudos
Reply