Hi,
We worked on the following platform:
1.Android 4.0.4(android-13.5.0-ga.01);
2.CPU:Freescale i.MX 6SoloLite EVK Board;
3.Codec: WM8960;
4.Bootup from SD card +LPDDR2;
5. Now the situation is:
Codec had been registered,but I can't hear any sounds when I play mp3 music.it is no voice on headphone.
6.Here is the source codes:
6.1).Board files configuration of WM8960:
static struct imx_ssi_platform_data mx6sl_evk_ssi_pdata = {
.flags = IMX_SSI_DMA | IMX_SSI_SYN,
};
static struct mxc_audio_platform_data wm8960_pdata;
static struct platform_device mx6sl_evk_audio_wm8960_device = {
.name = IMX_WM8960_DRIVE_NAME,
};
static struct wm8960_data wm8960_config_data = {
};
static int wm8960_clk_enable(int enable)
{
imx6Sl_debug("enable=%d",enable);
if (IS_ERR(extern_audio_root)) {
pr_err("audio clock source is not found!\n");
return -1;
}
if (enable)
clk_enable(extern_audio_root);
else
clk_disable(extern_audio_root);
return 0;
}
static int mxc_wm8960_init(void)
{
struct clk *pll4;
int rate;
imx6Sl_debug();
extern_audio_root = clk_get(NULL, "extern_audio_clk");
if (IS_ERR(extern_audio_root)) {
pr_err("can't get extern_audio_root clock.\n");
return PTR_ERR(extern_audio_root);
}
pll4 = clk_get(NULL, "pll4");
if (IS_ERR(pll4)) {
pr_err("can't get pll4 clock.\n");
return PTR_ERR(pll4);
}
clk_set_parent(extern_audio_root, pll4);
rate = clk_round_rate(extern_audio_root,11289600);
clk_set_rate(extern_audio_root, rate);
imx6Sl_debug("rate =%d",rate);
wm8960_pdata.sysclk = rate;
return 0;
}
static struct mxc_audio_platform_data wm8960_pdata = {
.ssi_num = 1,
.src_port = 2,
.ext_port = 3,
.hp_gpio =-1,
.hp_active_low = 1,
.mic_gpio =-1,
.mic_active_low = 1,
.init = mxc_wm8960_init,
.clock_enable = wm8960_clk_enable,
};
static int __init mx6_evk_init_audio(void)
{
imx6Sl_debug();
mxc_register_device(&mx6sl_evk_audio_wm8960_device,
&wm8960_pdata);
/*imx-ssi.c*/
imx6q_add_imx_ssi(1, &mx6sl_evk_ssi_pdata);
return 0;
}
6.2).WM8960.c and imx-wm8960.c please see attachment files(wm8960.txt,imx-wm8960.txt).
7. The log of wm8960 can see this log(wm8960_log_0122.txt).
Can you tell me where was wrong ?
Thanks very much in advance.
Original Attachment has been moved to: wm8960.txt.zip
Original Attachment has been moved to: wm8960_log_0122.txt.zip
Original Attachment has been moved to: imx-wm8960.txt.zip
You can do following.
- review platform interface code. Which does the configuration for SSI.
- Verify signal on SSI using Scope.
In Audio clock is important part. You should verify that first.
Check MCLK, LRCLK and Bit clk.
Thanks
Saurabh
Hi,Saurabh,
The Audio clock is 11289600,I had set,but it only get the 10156249.
In other codec,for example, TLV320AIC3206IRSBR,it also get the 10156249,but it works very,
so I think the Audio clock is right,so the MCLK is right.
Thanks.