Voltage select for GPIO's

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Voltage select for GPIO's

1,081件の閲覧回数
samikshadubey
Contributor I

Hi All,

I am working on IMX6 sololite Processor with ltib setup.I am facing voltage select issue for GPIO's .The voltage level for GPIO's is selected 1.8v and the required voltage is 3.0v.

Can anyone please help that what changes should we need in Board file (ltib/rpm/BUILD/linux-3.0.35/arch/arm/mach-mx6/board-mx6sl_evk.c) ?

ラベル(1)
0 件の賞賛
返信
1 返信

822件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

changes can be done in register Pad Control Register IOMUXC_SW_PAD_CTL_PAD_xx_yy

LVE field in:

linux/arch/arm/mach-mx6/board-mx6sl_evk.c

using sect.2.3.1 Defining the Pads Porting Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信