Voltage of USB OTG DP pin of i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Voltage of USB OTG DP pin of i.MX6

806件の閲覧回数
宗標廖
Contributor V

Hello,Community

I have an issue about the voltage of USB OTG DP pin of i.MX6.

In normal case, the DP pin should have a voltage change as bellow when the kernel is starting up.

※I measured it on i.MX6DLSabreAuto and connected the OTG port to PC.

But my customer met an problem. On their board, after the D+ pin rising to 0.6V, it will not fall down

and keep on 0.6V for ever.

Could you give me some advice to analyze the reason?(I think it is something about kernel,but I have not find it)

usb_otg_dp_0_6.png

Best Regards,

ZongbiaoLiao

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

690件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

main points for check USB_LDO (VDD_VBUS_CAP) voltage,

24MHz signal quality and possibility of ESD damage. It may be useful

to check sect.3.14 i.MX6 System Development User’s Guide (rev.1, 6/2013)

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

690件の閲覧回数
宗標廖
Contributor V

Hi Igor

Please help me!

Thank you very much!

0 件の賞賛
返信

690件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

behaviour of usb signals is described in USB 2.0 specificaion

USB.org - Documents

Best regards

igor

0 件の賞賛
返信

690件の閲覧回数
宗標廖
Contributor V

Hi Igor

Thank you for your reply!

In normal case,why does OTG D+ pin have a voltage change as above(why does it need this)?

Please explain the reason.

Best Regards,

ZongbiaoLiao

0 件の賞賛
返信