Voltage of USB OTG DP pin of i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Voltage of USB OTG DP pin of i.MX6

765 次查看
宗標廖
Contributor V

Hello,Community

I have an issue about the voltage of USB OTG DP pin of i.MX6.

In normal case, the DP pin should have a voltage change as bellow when the kernel is starting up.

※I measured it on i.MX6DLSabreAuto and connected the OTG port to PC.

But my customer met an problem. On their board, after the D+ pin rising to 0.6V, it will not fall down

and keep on 0.6V for ever.

Could you give me some advice to analyze the reason?(I think it is something about kernel,but I have not find it)

usb_otg_dp_0_6.png

Best Regards,

ZongbiaoLiao

标签 (2)
0 项奖励
回复
4 回复数

649 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

main points for check USB_LDO (VDD_VBUS_CAP) voltage,

24MHz signal quality and possibility of ESD damage. It may be useful

to check sect.3.14 i.MX6 System Development User’s Guide (rev.1, 6/2013)

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

649 次查看
宗標廖
Contributor V

Hi Igor

Please help me!

Thank you very much!

0 项奖励
回复

649 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

behaviour of usb signals is described in USB 2.0 specificaion

USB.org - Documents

Best regards

igor

0 项奖励
回复

649 次查看
宗標廖
Contributor V

Hi Igor

Thank you for your reply!

In normal case,why does OTG D+ pin have a voltage change as above(why does it need this)?

Please explain the reason.

Best Regards,

ZongbiaoLiao

0 项奖励
回复