Vivantec GPU does not respond when iMX6Q operates with single core.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vivantec GPU does not respond when iMX6Q operates with single core.

823 Views
johnturnur
Contributor III

In SABRESDP(iMX6Q) is there a restriction to keep atleaset 2 core active to use GPU ?


I'm running an OpenGL application on core0. If I shutdown core1,core2,core3 GPU does not respond.


Labels (3)
0 Kudos
Reply
1 Reply

609 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, John

     As far as I know, there is no restriction between CORE number and GPU. BTW, when do you shutdown the core1, core2 and core3? Before you lunch GPU app or after? can you try to add "nosmp" or "maxcpus=1" in your uboot command line to let kernel boot up only one core then run the GPU?

0 Kudos
Reply