Vivante v5.0.11p7.4 GPU Driver with Profiler Enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vivante v5.0.11p7.4 GPU Driver with Profiler Enabled

787 Views
kannankathirvel
Contributor I

Hi.. I'm trying to enable the profiler option in order to measure the application's GPU utilization in the i.MX6. In this process, I need to change the config to include 

USE_PROFILER = 1 and 

USE_POWER_MANAGEMENT= 0 

and rebuilt the kernel with the GPU driver files with profiling options enabled. 

Do you know any idea on how to get the latest Vivante GPU driver files with Profiler options enabled? 

Or any information on profiling the application performance in i.MX6 will help.

0 Kudos
Reply
1 Reply

531 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kannan

for profiling one can try gpu tools :
IDE - Debug, Compile and Build Tools (15)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...
and community threads
https://community.nxp.com/message/407851
https://community.nxp.com/message/632272

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply