VPU: timestamps, and audio/video sync

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VPU: timestamps, and audio/video sync

1,458 次查看
PhilEndecott
Contributor II
Does anyone here know anything about the VPU? I have basic video playback working, and now I need to get audio-video sync correct. This is from an MPEG transport stream (DVB) and I believe that I need to use the Presentation Time Stamp (PTS) fields from the two PES streams for synchronisation. It is simple enough to feed the two streams into the two decoders in synchrony. Unfortunately this is insufficient, as the latency from writing to the VPU input buffer to getting a frame out is variable. According to the MPEG spec, the correct way to do this is to feed in the data to both audio and video decoders as it is received, and to fetch video frames and audio data out of the decoders in synchrony. The difficulty is that I don't know the PTS timestamps for the frames as they come out. Ideally, I think I'd like the VPU to report the corresponding PTS value in the DecOutputInfo struct, however this does not seem to be present. Has anyone else ever looked at this? (Are any of Freescale's VPU engineers reading this?) Thanks, Phil.
标签 (1)
0 项奖励
3 回复数

934 次查看
KanHU
Contributor III

it's under libs/me/ of gst-fsl-plugins package. It's a really simple algorithm.

I'm not look at ffmpeg code, but I think there should be some algorithm in that too for timestamp.

0 项奖励

934 次查看
PhilEndecott
Contributor II
Thanks for the reply. No, I'm not using a "multimedia framework". Can you point me to the source for this gstreamer algorithm? What you describe sounds like a bit of a hack.
0 项奖励

936 次查看
KanHU
Contributor III

Are you use some multimedia framework? like Freescale provide gstreamer plugins which can handle AV sync.

 

Currently VPU gstreamer plugins provided by Freescale handle the timestamp with some simple algorithm. The precondition is we get PTS for a frame based, and the plugin will hold a pool to hold the timestamp it received and get timestamp from the pool when a decompressed frame output, And there's some algorithm to reorder the timestamp or correct it since some of them are illegal values.

0 项奖励