Hello,
We are developing an i.MX6 SOM that is designed to have common hardware for the SOLO, Dual, and Quad processors. We need to increase LDO_SOC to 1.225 to operate the VPU above 264MHz. Two questions have arisen,
1 - We noticed that there seems to be mention of reducing DDR jitter if LDO_SOC is 2.275V is this important?
2 - We were considering increasing the VDD_SOC_IN to 1.45V to margin the input above the drop in the internal LDO. Is this reasonable?
Thanks for your help,
Best Regards,
BW
解決済! 解決策の投稿を見る。
Hi BOMS
1. in general the higher the voltage level on VDDSOC_CAP,
the less jitter. If there are jitter issues, an easy fix is to raise VDDSOC_CAP.
2. http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf Table 6. Operating Ranges footnote 4:
VDD_ARM_IN and VDD_SOC_IN must be at least 125 mV higher than the LDO Output Set Point for correct voltage regulation.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi BOMS
1. in general the higher the voltage level on VDDSOC_CAP,
the less jitter. If there are jitter issues, an easy fix is to raise VDDSOC_CAP.
2. http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf Table 6. Operating Ranges footnote 4:
VDD_ARM_IN and VDD_SOC_IN must be at least 125 mV higher than the LDO Output Set Point for correct voltage regulation.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for the quick reply.