VDD_CACHE_CAP ( Pad N12 ) in i.MX6 Duallite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VDD_CACHE_CAP ( Pad N12 ) in i.MX6 Duallite

980 Views
sreekn
Contributor I

The AN4397.pdf application note regarding common hardware for i.MX6 Solo, Duallite, Dual & Quad, says,

The third difference is about VDD_CACHE_CAP (N12). In i.MX 6Quad and i.MX 6Dual,

VDD_CACHE_CAP should be connected to VDDSOC_CAP, whereas in i.MX 6DualLite and

i.MX 6Solo, pin N12 can be NC.


Is it is OK to keep the N12 Pad connected to VDDSOC_CAP power supply for Duallite also, or whether it has to be mandatorily NC for Duallite & Solo ?

Labels (1)
0 Kudos
Reply
2 Replies

683 Views
Karthik37
Contributor I

Hi Sree,

Did you got the answer for the question posted. I am also looking for it.

Thanks,

Karthik R

0 Kudos
Reply

683 Views
sreekn
Contributor I

Hi Karthik,

I haven't got clarity on this yet. However I am following the SABREBOARD design, in which the VDDSOC_CAP is kept connected to the NC_N12 for Duallite version as well. Fingers Xed !!!

0 Kudos
Reply