Hi,
I'm trying to load the M4 binary after Linux boot, Linux bash doesn't respond when using RPMSG pingpong examples.
I made the following changes
diff --git a/arch/arm/mach-imx/src.c b/arch/arm/mach-imx/src.c index c53b6da411b9..9859751b5109 100644 --- a/arch/arm/mach-imx/src.c +++ b/arch/arm/mach-imx/src.c @@ -194,6 +194,7 @@ void __init imx_src_init(void) m4_is_enabled = true; else m4_is_enabled = false; + m4_is_enabled = true; val &= ~(1 << BP_SRC_SCR_WARM_RESET_ENABLE); writel_relaxed(val, src_base + SRC_SCR);
I tried to start the M4 binary in u-boot and everything worked as expected. Do I need to make any changes to the way I load the M4 binary using m4fwloader?
yocto version
repo init -u git://source.codeaurora.org/external/imx/imx-manifest.git -b imx-linux-zeus -m imx-5.4.24-2.1.0.xml
examples
FreeRTOS_BSP_1.0.1_iMX6SX.tar.gz
pop
Hi dddd
for m4fwloader issues one can post on
https://github.com/NXPmicro/imx-m4fwloader/issues
alternatively one can try m4ctrl
https://source.codeaurora.org/external/imxsupport/m4ctrl/tree/README.md
Best regards
igor