Using Yocto with IMX6ULL 14x14 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using Yocto with IMX6ULL 14x14 EVK

3,174 Views
mitchgaines0
Contributor I

I'm trying to build a yocto image for my IMX6ULL 14x14 EVK board by following this set of instructions:
https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf 

However, when building an image, only u-boot seems to start. U-boot then never seems to get to an autoboot step or allow access to the console. So, the kernel never starts. 

Here is my build configuration:

Build Configuration:
BB_VERSION           = "2.2.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "universal"
TARGET_SYS           = "arm-poky-linux-gnueabi"
MACHINE              = "imx6ull14x14evk"
DISTRO               = "fsl-imx-wayland"
DISTRO_VERSION       = "6.1-langdale"
TUNE_FEATURES        = "arm vfp cortexa7 neon thumb callconvention-hard"
TARGET_FPU           = "hard"
meta                 
meta-poky            = "HEAD:b50f718e4cb73214e7ad298484ecdadd6cfeb866"
meta-oe              
meta-multimedia      
meta-python          = "HEAD:c354f92778c1d4bcd3680af7e0fb0d1414de2344"
meta-freescale       = "HEAD:09c47379218167dda9fb0098129909a667fea2ec"
meta-freescale-3rdparty = "HEAD:96c1f6a6c2cad246687cd695e0873fcc6cdde935"
meta-freescale-distro = "HEAD:1069c2f210b18cd707a4d8a82140a684a42a4ff6"
meta-bsp             
meta-sdk             
meta-ml              
meta-v2x             = "HEAD:82c29a7fab71e5e9c5fc28af554c0289d0a00262"
meta-nxp-demo-experience = "HEAD:c057a681cf11923b22e16b9cdb0ad2b9187eced2"
meta-arm             
meta-arm-toolchain   = "HEAD:025124814e8676e46d42ec5b07220283f1bdbcd0"
meta-chromium        = "HEAD:e232c2e21b96dc092d9af8bea4b3a528e7a46dd6"
meta-clang           = "HEAD:22f1cc330d3501923d2dc27cd3fc424c69c3a73a"
meta-gnome           
meta-networking      
meta-filesystems     = "HEAD:c354f92778c1d4bcd3680af7e0fb0d1414de2344"
meta-qt6             = "HEAD:4f7d02004cd78f0fca77489deb7487bfb301ea36"
meta-parsec          
meta-tpm             = "HEAD:2aa48e6f4e519abc7d6bd56da2c067309a303e80"
meta-virtualization  = "HEAD:8857b36ebfec3d548755755b009adc491ef320ab"

 

I have attempted to build core-image-minimal, imx-image-core, and imx-image-multimedia. All of these result in the same problem. Here is the console output from u-boot:

U-Boot 2022.04-lf_v2022.04+g7376547b9e (Mar 01 2023 - 07:35:40 +0000)

CPU:   i.MX6ULL rev1.1 792 MHz (running at 396 MHz)
CPU:   Industrial temperature grade (-40C to 105C) at 47C
Reset cause: POR
Model: i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM:  512 MiB
Core:  65 devices, 18 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (480 x 272)
        [0] lcdif@21c8000, video
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc1(part 0) is current device
flash target is MMC:1
Net:   Could not get PHY for FEC1: addr 1
Could not get PHY for FEC1: addr 1
Get shared mii bus on ethernet@2188000

After that, it seems to just hang with no access to the uboot console

When the system boots from the emmc (with what was shipped on the board), a kernel seems to start.

Any indication on what I need to do here? 

Labels (3)
2 Replies

3,013 Views
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @mitchgaines0 ,

Sorry for the late response. Please help me with the following questions to pinpoint the root of your problem:

1. What BSP version are you trying to build?

2.What process are you following to flash your created image? 

3. To what device are you flashing to? 

4. From which OS are you flashing from?

Thank you.

Best regards,
Hector.

0 Kudos
Reply

3,067 Views
felix1
Contributor IV

Hi,

I build yocto image follow the URL

https://github.com/nxp-imx/meta-matter#how-to-build-the-yocto-image-with-integrated-openthread-borde...

It boots success. Maybe you can check the differences with yocto user guide, just for your reference.

0 Kudos
Reply