Hi,
I'm using i.MX 8M Mini Processor.
I cannot use UART3_TXD (GPIO5[27]) as an GPIO.
What could be the problem?
Best regards,
Adde
解決済! 解決策の投稿を見る。
Hi Adde
reason may be that it is used by other driver/application. One can try to set manually
using jtag debugger or memtool
https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=lf-5.10.72_2.2.0
Another reason may be that chip is broken, probably due to ESD or overheating.
Best regards
igor
see
Hi Adde
reason may be that it is used by other driver/application. One can try to set manually
using jtag debugger or memtool
https://source.codeaurora.org/external/imx/imx-test/tree/test/memtool?h=lf-5.10.72_2.2.0
Another reason may be that chip is broken, probably due to ESD or overheating.
Best regards
igor
Hi Igor,
Thanks for your previous answer.
What about this post?
https://community.nxp.com/t5/i-MX-Processors/Using-UART3-TXD-GPIO3-24-as-an-GPIO/m-p/375613
Could it be the same problem I am experiencing?
Best regards,
Adde
>What about this post?
that post talks about UART3_TXD which is connected to external part
and that part(configured as output) drives UART3_TXD.
Best regards
igor