Using Mfgtool to flash eMMC in iMX6DL-SDB boards.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using Mfgtool to flash eMMC in iMX6DL-SDB boards.

1,068 Views
kaarkuzhalimuru
Contributor I

I tried to flash the eMMC of the iMX6DL sabresd board through Mfgtool and I am facing an error.

The steps I followed are:

  1. Copying the images to the 'Profiles/MX6DL Linux Update/OS Firmware/' directory
  2. Updating the cfg.ini file
  3. Connecting the board to PC.
  4. Run the Mfgtool2. It detects the HID-Compliant device.
  5. Pressing 'Start' button to download.
  6. It fails while accessing boot partition.
  7. The error on terminal is:

 pastedImage_1.png

I have attached the cfg_ini file and mfgtool log file.

Labels (1)
0 Kudos
3 Replies

861 Views
joanxie
NXP TechSupport
NXP TechSupport

what mfgtool verion do you use? you can choose the specific .vbs file for EMMC for your board, if you don't know which one, pls tell me what's your bsp version

0 Kudos

861 Views
kaarkuzhalimuru
Contributor I

Hi, I am using mfgtool2 (Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER).

0 Kudos

861 Views
joanxie
NXP TechSupport
NXP TechSupport

where did you download this mfgtool? I suggest that you can download from the link as below:

i.MX 6DualLite Applications Processors | Dual Arm® Cortex®-A9 @1GHz |NXP 

the latest version is "IMX6_L4.1.15_1.0.0_MFG_TOOL",

then you can choose the "mfgtool2-android-mx6dl-sabresd-emmc.vbs" for your board, refer to your cfg file I don't see the mmc=?, if you couldn't open .vbs file, you can set the cfg according to this vbs file.

0 Kudos