User board LED on i.MX 6SX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

User board LED on i.MX 6SX

415件の閲覧回数
mmmtq2011
Contributor I

Hi,

I'm new at NXP, I just received the i.MX 6SX, and I've been looking at the schematics to check if there are any user LEDs on the board, because I want to test a program that blinks the LED when I press the function pushbuttons, but it looks that they are no any accessible LEDs on the board. 

I've checked the linux sysfs and I've found three mmc LEDs inside this path: /sys/class/leds/ but when I toggled any of them none of the LEDs on the board are toggled. 

so my question is: is there any user LED on i.MX 6SX board?

Best Regards,

Mohammed

ラベル(1)
0 件の賞賛
1 返信

352件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mohammed,

There are no user LEDs which can be used trough GPIOs on the i.MX6SX SABRE board (I’m assuming this is the board you have received from NXP but please double check that this is the case). You may find the schematics on the web to see how the LEDs are routed but I’m afraid it wasn’t designed with this feature in mind.

My apologies for the inconvenience.
Regards,

0 件の賞賛