Use DDR3L(16bit) Single chip to Connect the i.MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use DDR3L(16bit) Single chip to Connect the i.MX6SL

617 Views
tony_l_cai
Contributor III

Hi,Community,

          Can I use DDR3L(16bit) single chip to connect the i.MX6SL,not to combine the double chips to 32bit,then connect the DDR controller(32 bit).

Can I? if I can, which settings I need in SW or HW ?  Thanks!

Labels (3)
Tags (2)
0 Kudos
1 Reply

378 Views
Yuri
NXP Employee
NXP Employee

   Yes, DDR3L 16 bit mode is supported, according to the Reference Manual :
MMDC is a multi-mode DDR controller that supports DDR3/DDR3L x16/x32.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos