Use DDR3L(16bit) Single chip to Connect the i.MX6SL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Use DDR3L(16bit) Single chip to Connect the i.MX6SL

632 次查看
tony_l_cai
Contributor III

Hi,Community,

          Can I use DDR3L(16bit) single chip to connect the i.MX6SL,not to combine the double chips to 32bit,then connect the DDR controller(32 bit).

Can I? if I can, which settings I need in SW or HW ?  Thanks!

标签 (3)
标记 (2)
0 项奖励
1 回复

393 次查看
Yuri
NXP Employee
NXP Employee

   Yes, DDR3L 16 bit mode is supported, according to the Reference Manual :
MMDC is a multi-mode DDR controller that supports DDR3/DDR3L x16/x32.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励