[Urgent]Question about Reducing power consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Urgent]Question about Reducing power consumption

799件の閲覧回数
ko-hey
Senior Contributor II

Hi all

We are considering reducing SOC and ARM power consumption.
I would like to change the clock root frequency of AXI, AHB, IPG from the information written in the Reducing Power Consumption of page 5 of AN 5383, but I can not boot with either fix.

Q1
There seems to be some limitation on the clock root frequency of AXI, AHB, IPG, but can you give me relevant information?

Q2

When entering Wait mode or Deep sleep mode, we have to adjust the frequency of the above 3 clocks.

Is there any change procedure and sample source code ?

Ko-hey

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

697件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  recommended configurations are provided in NXP Linux BSP, please use

sections 2.3.3 [CPU Frequency Scaling (CPUFREQ)] and 2.3.4 (Dynamic Bus Frequency) of

recent i.MX_Linux_Reference_Manual.pdf.  The documentation contains information where working

points and source codes may be found.   

Recent BSP doc package :

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Summary Page :

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

697件の閲覧回数
ko-hey
Senior Contributor II

Hi Yuri

Thank you for quick reply.

Maybe the section which you mentioned is section 23 and 24.

Am I correct ?

Ko-hey

0 件の賞賛
返信

697件の閲覧回数
Yuri
NXP Employee
NXP Employee

I meant the recent doc package. It has slightly different structure.

Regards,

Yuri.

0 件の賞賛
返信

697件の閲覧回数
ko-hey
Senior Contributor II

Yuri

I understand.

Thank you.

Ko-hey

0 件の賞賛
返信