Hello, AEs:
We use the SAI interface to connect an LMX2571, we want to send data to LMX2571 through this interface, like SPI or Uart drivers, open a device, call IOCTL command to configure I2S, and then send data. Is there any way to support this? I am not familiar with the audio architecture, and out project is very urgent, I hope to get your effective support. thanks.
Hi 国承 张
one can look at non-linux SAI MX6ULL FreeRTOS SDK examples below
and develop own SAI interface, using SPI or Uart drivers IOCTLs as examples:
Welcome | MCUXpresso SDK Builder
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------