Hello,
I've made a construction with iMX6 solo based on the Sabre SD development board. It looks like I'm not going to need some regulators from the PF0100, for instance VGEN1 and VGEN2. I assume their outputs should just be NC then? Also, this implies that I do not need to connect any supply to VIN1 (which powers VGEN1 and VGEN2). Is this correct? Can I just leave VIN1 unconnected and connect VIN2 and VIN3 only?
BR,
Emil
解決済! 解決策の投稿を見る。
Please refer to Table 1 (MMPF0100 Pin Connection Guidelines) of AN4717
(Schematic Guidelines for the MMPF0100).
http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf
Please refer to Table 1 (MMPF0100 Pin Connection Guidelines) of AN4717
(Schematic Guidelines for the MMPF0100).
http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf