Unused DQ pins of i.MX6S

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unused DQ pins of i.MX6S

ソリューションへジャンプ
968件の閲覧回数
torus1000
Contributor V

Hi all,

I believe i.MX6S and i.MX6DL has same pins but i.MX6S only supports 32b DDR3.

Is it OK to leave unused DQ pins open?

Thanks.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
774件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

yes it is OK. In general it may be useful to look at

AN4397  Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
775件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

yes it is OK. In general it may be useful to look at

AN4397  Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信