Unable to flash code over Device "MIMXRT1052XXXXB".

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to flash code over Device "MIMXRT1052XXXXB".

698 Views
niket_zope
Contributor III

I have Device "MIMXRT1052XXXXB" whenever is try to connect it via Jlink utility either

JFlash or Jlink commander recieve the following error. It would be very helpful if some can help to resolve the issue.

 

Note: i tried connecting and unlocking the kinetis but it throws an error stating

J-Link>unlock kinetis
Found SWD-DP with ID 0x0BD11477
Unlocking device...ERROR: Read from DP/AP register failed!

 

While flashing the srec it shows this !  

niket_zope_0-1638275289490.png

@jeremyzhou @alex_rodriguez  @Hui_Ma 

 

 

0 Kudos
Reply
2 Replies

604 Views
niket_zope
Contributor III

hi @jeremyzhou , I am using the custom board having MIMXRT1052xxx6B processor connected to it. I am getting the following error when i am trying to read back or even to flash any binary in external flash at location 0x60000000 

 

niket_zope_1-1650602890372.png

 

0 Kudos
Reply

691 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before giving some advice, I'd like to know which board you used for testing.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply